Is there a way in a
Turning Operation to add chip break moves into a cut? This would be done by dividing long tool motion into a series of short moves and than adding a dwell to the path. Adding these small moves with the dwell command will cause the tool to pause so that the chip can be broken into small pieces. How can this type of motion be added?

Solution
The
Local Return option can be used to add this tool motion. The path settings might look something like the picture below when done.

The output might look something like the picture below. Notice the
G4 dwell commands after each short
Z move.

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1903
Function: TURNING
Ref: 002-8016880