Retract Distance for X, Y, and Z are not seen in the Cycle Parameters dialog box.



Solution
Add the following line to the
"ude.cdl" file and then close and re-open NX for these to see the
"Retract Distance" parameters.
# Remove the # from the INCLUDE statement to enable Siemens 840D cycle parameters to Hole Making and Manual Hole Making operations.
Start of ude.cdl file is below...
MACHINE FANUC
INCLUDE {$UGII_CAM_USER_DEF_EVENT_DIR/Siemens_Cycles.cdl}

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1899
Function: USER_INTERFACE
Ref: 002-8016842