Solid Edge Solid Edge Embedded Client Structure Editor does not show Inter-part Links

2021-10-06T23:56:47Z
DOC_MANAGEMENT

Summary


Details

In Solid Edge ST10 I try to do a "Save as" of an assembly using Structure Editor.  A few child items from this assembly have Inter-part Links.  These links are not displayed in the source BOM-view (left upper panel). 

In the previous Solid Edge version (ST9) we could control the check on the reverse link with a registry key:
 
HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\version 109\DEBUG\SEEC_SESE_Expand_ReverseLink

By default it is OFF (0) 

This registry switch does not exist for Solid Edge ST10.  After adding it manually the required links did not appear either.  Has the behavior been changed in Solid Edge ST10? 



Solution

We have stopped honoring this registry switch and now the behavior is to not expand reverse links.  If the reverse link is in context (BOM) then it will be shown, otherwise it will not be shown.  This behavior is effective from Solid Edge ST10 onwards.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 2016
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP12
Function: SEEC

Ref: 001-9664388

KB Article ID# PL8016826

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC