Import Assembly into Teamcenter - Item Type doesn't default to custom item type

2021-10-06T23:27:34Z

Summary


Details

Setting the customer defaults for "Import Assembly Into Teamcenter" to use a custom item type is not working.

There is a custom item type named "Gtac Item"; entered this name into Customer Defaults> Teamcenter Integration > Import/Export Assembly > Import tab : Item Type. 

Restart NX and launch the Import Assembly Into Teamcenter command; the Item Type value is not picking up from Customer Defaults.


* Reset the dialog did not help*, setting Teamcenter preference "TC_part_types_display_filter" did not help.

Solution

Use BMIDE to find out the "Name" and "Display Name" of that custom item type.

If unable to access BMIDE, use View Properties on an existing item of that custom item type.

The field for Multifield Key Information will list out "object_type=", this is the "Name".

This "Name" should be the string to use in Customer Defaults > Teamcenter Integration > Import/Export Assembly > Import tab : Item Type 

In this example case, this custom item type: 
Name: g333gtac
Display Name: Gtac Item 

The Customer Defaults should use g333gtac



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1851
Function: CLONE_IMPORT

Ref: 001-9665707

KB Article ID# PL8016797

Contents

SummaryDetails

Associated Components