Translations from NX to JT with nxtopv.exe fails when multifield-key is used

2021-10-06T23:27:34Z

Summary


Details

The syntax is not clear, how to export Multi Field Key (MFK) Items from Teamcenter using ugtopv.exe.

e.g.:

ugtopv.exe -pim=yes @DB/%MFK#%,=item_id=itemidx,object_name=objectnamex/A

will show an error in the command prompt: "Error 1140 :Failed to load part:" 

if you want to export Multi Field Key (MFK) Items from Teamcenter with ugtopv.exe



Solution

Right click in Teamcenter on the MFK Item you want to export-> View Properties

Use the content of PartIdentifier as input. Regardless of definition always the object_type (which is the Item type in this case) is also necessary with ugtopv.exe -pim=yes as a command line option.

(ug_clone would also work without object type).

Example:
If MFK is defined with ITEM ID and Object_name in Teamcenter BMIDE, the command in TC command shell would be:

ugtopv.exe -pim=yes @DB/%MFK#%,=item_id=itemidx,object_name=objectnamex,object_type=itemtypex/A

Notes and References

https://docs.plm.automation.siemens.com/tdoc/nx/1899/nx_help/#uid:xid913098

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Function: NX_JT

Ref: 002-8016790

KB Article ID# PL8016790

Contents

SummaryDetails

Associated Components