Details
What does the Auto-Scale Sketch command do?
Solution
Driving dimensions control the size and location of a sketch. The Auto-Scale Sketch command automatically scales a 2D or 3D sketch that contains just one driving dimension. When you place the first driving dimension that measures distance, radial, diameter, or symmetric diameter, and then you change its value, the whole sketch is scaled proportionally. You can scale the sketch by increasing or decreasing the value of the driving dimension as many times as needed. Auto-scaling continues until you deselect the option on the ribbon or add a second driving dimension.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V220.0
Function: DIMENSIONS
Ref: 002-8016750