Details
What is the Heal Mesh Faults option in the STL Import Options used for?
Solution
This specifies that you want to repair any mesh faults when you open the STL file. There is also a corresponding Heal mesh faults parameter in the SESTL.ini file, which is set to off by default. Leaving the parameter set to off only fixes basic faults, such as degenerative facets or duplicate vertices. Setting the value to on is a time consuming operation that fixes the basic faults, along with more complex faults, such as self-intersection faults.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V220.0
Function: STL
Ref: 002-8016748