Unable to move hole in Synchronous sheetmetal part
2021-10-06T23:56:42Z
Summary
Details
I have a Synchronous sheet metal part which contains a chamfered threaded hole. If I try and move this hole using the steering wheel, I am unable to do so and I get an error message.
These are the Hole Options used:
Solution
When 'Thread Extent' is set to 'Finite extent' and its value (2.00 mm in this case) is greater than the sheetmetal thickness (1.50 mm in this case) you will be unable to move the hole. The workaround is to change 'Thread Extent' to the 'To hole extent' option. Now you will be able to move the hole.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: SOLID_EDGE Application: PART/SHEETMETAL Version: V220.0 Function: SYNC_EDIT