Details
When creating a UDF with TCIN, the item name is automatically created with "UDF :: Name".
Is there any way to change creating colon "::"?
Solution
UDF prefix can have only 2 options ie colon "::" or underscore "__".
By default colon "::" appears.
To use underscores instead of colons, set the following environment variable.
"UGII_UDF_PREFIX_WITH_UNDERSCORES".
The environment variable can be set to "1", "yes" or "true".
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: UDF
Ref: 002-8016686