NX manager failed to launch with below error

Solution
If you are running Teamcenter Integration in the Teamcenter Secure Socket Layer (SSL) environment and if
environment variable "TEAMCENTER_SSL_CERT_FILE" is not set then the above error appears.
set the following environment variable before running NX. Set the variable to the same certificate file that is used for Teamcenter SSL setup. Ensure you use the fully qualified host name in the URL for the connection.
TEAMCENTER_SSL_CERT_FILE=<certificate file name (<filename>.pem) and path>
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: STARTUP
Ref: 002-8016685