NX Is it possible to specify specific "roll" while printing from NX?

2021-10-06T23:27:34Z
NX System Administration

Summary


Details

When printing from NX paper size can be specified but roll can't.
For example when setting paper to "roll 1" and film to "roll 2" everything gets printed from either paper from "roll 1" or film from "roll 2" when we want it to print to the specified roll.


HP DesignjetT1300 exists in the list of available plotters but we can't print with this plotter via the printer server and we had to use PDL converter to print from this plotter.




Question:
1. Given the situation above is there a way to print with "HP DesignjetT1300" without using PDL converter?





Solution

The HP T1300 is from the same family as the HP T1100 with the default configuration.
This should work out of the box with no need for custom configuration without using PDL converter.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1709
Product: NX
Application: GATEWAY
Version: V11.0.2
Function: PLOTTING

Ref: 002-8016655

KB Article ID# PL8016655

Contents

SummaryDetails

Associated Components

Plotting