NX Where should I set the font mapping when exporting PDF?

2021-10-06T23:27:34Z
NX for Design

Summary


Details

The cgmdef.txt file mentions "The cgmdef.txt file specifies the defaults used to create CGM files for File-> Export CGM and File-> Export PDF and NX Open functionality."
Does that mean that font mapping is not possible?
Where should I set the font mapping when exporting PDF?





 



Solution

The cgmdef.txt was intended mainly for CGM Export/Import. 
 For PDF Export, the mapped fonts are hidden only for the purpose of text search.  To make the "mapped" hidden text visible when using the cgmdef.txt file, please turn on the following environment variable:
 set UGII_PDF_NO_HIDDEN_TEXT=1
 Also, the variable UGII_ROOT_DIR is obsolete since NX11. The cgmdef.text is now in:%UGII_BASE_DIR%\ugii\



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: GATEWAY
Version: V11.0.2
Function: PDF

Ref: 002-8016654

KB Article ID# PL8016654

Contents

SummaryDetails

Associated Components

Modeling