How to change/edit material for multiple plates (or other Steel Feature) in detail design?

2021-10-06T23:27:33Z

Summary


Details

How to change/edit material for multiple plates in Ship Design / Ship Structure Detail Design? 



Solution

You can use "Paint Parameters" to set parameter for multiple plates the same as 1 "Source Plate". 
With "Paint Parameters" you can change all parameters of multiple plates (or other Steel Feature) at once.

Procedure: 
  1. Change 1 plate to the required stock parameters (if not available yet);
  2. Start "Paint Parameters"

  • Select Source Object: Plate with the required stock parameters (step 1);
  • Select all plates which need the same parameter applied (Target Objects) 
    This way all Target Objects will inherit the same parameters as the Source. Inheritance is "all or nothing". You cannot change just 1 parameter. 




Notes and References

Remark:
Paint Parameters can be applied to many Steel Feature objects as listed below: 
  • Plate
  • Stiffener/Edge Reinforcement 
  • Profile Cutout 
  • End Cut
  • Cutout
  • Corner Cut
  • Along Guide Cut
  • Edge Cut
  • Bracket
  • Collar Plate
  • Standard Part
  • Weld Joint
  • Excess Material (Manufacturing)


See Tdoc: Design (CAD) --> Ship Structure --> Common tools --> Paint Parameters 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SHIP_DESIGN
Version: V12.0
Function: STEEL_FEATURES

Ref: 001-8437419

KB Article ID# PL8016653

Contents

SummaryDetails

Associated Components