Maintenance Pack 14 for NX 12.0.2 is now available

2021-10-07T00:08:47Z

Summary


Details

Dear Siemens Customer,

Maintenance Pack 14 for NX 12.0.2 is now available on the Siemens Download Server.

NX 12.0.2 MP14 is an accumulation of fixes built for installation on top of Windows 64-Bit image of NX 12.0.2.

To select the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window:

      https://download.industrysoftware.automation.siemens.com/download.php

      Note: A valid WebKey account is required.

From the Full Product Download page, Enter "12.0.2.mp14" (including the quotes) in the Search box to see a list of links to the release letter and available release packages. 

Alternatively, the release packages can be found in the file navigator by selecting 'NX' from the Product Filter on the left of the webpage and then navigating through the directory structure by selecting: "NX Support > NX Supported > NX 12 > Maintenance-packs > Windows (64-bit)".


Sincerely, 

Siemens Digital Industries Software

SFB-NX-8016633
Product Information:
  • Product: NX

KB Article ID# PL8016633

Contents

SummaryDetails

Associated Components