NX 1872 Series Maintenance Software Fix (NX 1892.2940) is available for download

2021-10-07T00:08:47Z

Summary


Details

Dear Siemens Customer,


We are pleased to inform you that the latest NX 1872 Series Maintenance Software fix is now available for download from the Siemens PLM Download Server.


Please disregard this announcement if you are on the current NX 1899 Series.


Note:  Automatic updates will not be available for releases on NX 1872 Series after NX 1892, including NX 1892.2940. Users who are on NX 1892 with automatic update option turned on will be notified to download and install the NX 1899 release. If any release on the NX 1872 Series is preferred, users must download the release from the GTAC Download Server.
 
Download of NX on Windows 64-bit

 
Please use the following steps to download the NX product release and its documentation.
Note: A valid WebKey account is required. 


  • In your browser's address field enter the URL: https://download.industrysoftware.automation.siemens.com/
    Login using your WebKey username and password
     
  • From the Download page, enter "SiemensNX-1892.2940_wntx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages.  
       
  • Alternatively, the NX product release can be found using file navigator by entering NX into the Product Filter feature on the left of your browser and then navigating through the NX directory structure as follows:  
    • Expand the "NX Support" folder 
    • Expand the "NX Supported" folder 
    • Expand the "NX 1872 Series" folder 
    • Expand the current release folder (NX 1892.2940)   
       
  • To download the NX product:     
    • Right click on the Release Package file(s) 
    • Select "Save Target As" or "Save Link As" to save the file(s) to your local destination 

  • Note: The only upgrade option available for this NX 1872 Series Maintenance Software Fix is an MSI-based installer, which is designed to update (upgrade) existing NX installations or allow the base install of this NX release if NX is not previously installed on a system. The release can be downloaded as a single file:
    • SiemensNX-1892.2940_wntx64.zip

  • To download the NX documentation:  
    • Expand the "NX Support" folder 
    • Expand the "NX Supported" folder 
    • Expand the "NX 1872 Series" folder 
    • Expand the current release folder (NX 1892.2940)   
    • Expand the "Documentation" folder 
    • Right click on the product documentation link 
    • Select "Save Target As" or "Save Link As" to save the file to your local destination. 
In all cases, please refer to the supplied README file for installation instructions. 


If you encounter any problems during this installation, please contact your local Siemens Digital Industries Software support office.
   
For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:
 
         NX:   http://www.plm.automation.siemens.com/en_us/products/nx/
         GTAC:   https://www.plm.automation.siemens.com/global/en/support/ 


 


Sincerely,


Siemens Digital Industries Software 

SFB-NX-8016628
Product Information:
  • Product: NX

KB Article ID# PL8016628

Contents

SummaryDetails

Associated Components