File translation error while exporting draft to pdf file format.

2021-10-06T23:56:40Z

Summary


Details

When user trying to export draft to Adobe Acrobat document (*.pdf) file format, getting error as the draft could not be saved because of a file translation error.

Solution

This issue seems to be due to the 'printerinstaller.exe' was not completely installed and the printer Solid Edge Velocity PS printer might be missing or not default.
 
 - Please check if 'Solid Edge Velocity PS Printer 2.0' is available in Printer and Scanners list.
 - If it is there, please select it and make it as a default printer.
 - If the 'Solid Edge Velocity PS Printer 2.0' is not listed in Printer and Scanners, then please install it using 'PrinterInstaller.exe' from Solid Edge program folder.




Notes and References

9622581

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V110.0
Function: PDF

Ref: 002-8016619

KB Article ID# PL8016619

Contents

SummaryDetails

Associated Components