Details
User has created alternate assembly. He wants to place the alternate positions in draft but the option to select the position does not appear. The option "Set primary and Alternate positions" is not active.
Solution
Please check you might have used 'Create a Family of Assemblies' option in Alternate Assemblies while creating members.
* Create A Family Of Assemblies
- Specifies that you want to create a family of assemblies.
If you use 'Create Alternate Positions Of The Assembly' while creating Alternate assemblies menders, it will show option to select the position to 'set Primary and Alternate position' while creating drawing view in draft.
* Create Alternate Positions Of The Assembly
- Specifies that you want to create alternate positions of the assembly.
Notes and References
9642003
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1507
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V220.0
Function: COMPONENTS
Ref: 002-8016616