Explosion on Drawing not possible

2021-10-06T23:27:33Z

Summary


Details

An Explosion View should be transferred to a Drawing sheet.
The Exploded views are from a Master Model.
The new view is created from Explosion in Part Navigator and should be 
transferred to the Drawing sheet.
The Problem is that the Explosion view will not be created as exploded view.

Solution

Exploded views from master model is currently not supported. 
The work around is to create the exploded views in the drawing file. 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V12.0.1
Function: DRAWING/VIEW

Ref: 002-8016573

KB Article ID# PL8016573

Contents

SummaryDetails

Associated Components