Custom Symbol Library Installation issue.

2021-10-06T23:27:33Z

Summary


Details

If user not able to install Custom Symbol libraries in Native NX.


May be due to security reason or access issue in unzip Custom Symbols folder in C drive or running a Custom_Symbol-Installation.bat file.



Solution

Workaround:                                 


1. Copy Install tool folder other Drive.


2. Unzip tool.zip folder.


3. Double click Custom_Symbol-Installation.bat to start the installation.


If .bat file can't run , unzip Custom Symbols.zip file.


4. Define path of the custom symbol folder in Customer Defaults>>Gateway>>reuse library>>Symbols Library in Native NX.



Notes and References

9648735

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1847
Function: SYMBOL

Ref: 002-8016542

KB Article ID# PL8016542

Contents

SummaryDetails

Associated Components