Last Saved Property is not available for Callouts

2021-10-06T23:56:38Z

Summary


Details

Due to the fact that the Last Saved Property is not available in a Callout, the property %{Accessed} is used instead.  However this date is changed every time the Draft file is opened.  Why?



Solution

It is correct that the %{Accessed} property is changed every time as the "Date accessed" contains the date and time of the last file access (whether read or executed).  Therefore when the file is opened it is accessed and consequently the date is changed. 

We recommend using the %{Modified} property, which refers to the "Date Modified" Property when the "Last Saved" Property is requested.  However it important to know that the "Modified" property could also be changed outside of Solid Edge e.g. by a modification in the Windows Explorer Properties. 

An Enhancement Request exists for adding the Last Saved Property in a Callout.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1903
Product: SOLID_EDGE
Application: DRAFT
Version: V219MP10
Function: ANNOTATIONS

Ref: 001-9625145

KB Article ID# PL8016534

Contents

SummaryDetails

Associated Components