Details
When set SEEC_SaveAs_New_ItemType to 1 and perform "SaveAs" on SESE, all target objects are created as New regardless of whether the Item Type has changed.
Solution
This issue is working as designed.
This is similar to Save As new item type in SEEC.
When this preference is enabled, Save As will create an entry on the right side of SESE. This entry will have the same Item Type as the source. The user can expand the list of available Item Types and select a different Item Type. This will invoke the same behavior as the Save As New Item Type in SEEC.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP2
Function: SEEC
Ref: 002-8016509