Issue while check in Standard Parts in Solid Edge managed mode

2021-10-06T23:56:36Z

Summary


Details

Cannot generate this part.
The operation input descriptor *XXXXXXX* requires a value for the property *xxxxxxxx* for business objects of type *XXXXXX*.



Solution

This issue occurs when custom property (real name) and it's value is not inputted while generating standard part, to overcome this follow below steps.

Select a component from standard part admin. From RMB menu Add Custom Properties 


add the custom property and its value here, then generate and try to place same part in Solid Edge.


Select another component and then add the custom property and its value here, this time place component in Solid Edge and have generated while placing.


Ensure use correct property name and its value.
Can cross verify from cpd.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP10
Function: SEEC

Ref: 002-8016507

KB Article ID# PL8016507

Contents

SummaryDetails

Associated Components