Solid Edge Is it possible to perform Save and Upload Operation using single Save Operation in SEEC

2021-10-06T23:56:36Z
DOC_MANAGEMENT

Summary


Details

In Solid edge with Teamcenter integration mode, after changed drawing user need to press save button to save and than go to Manager > Upload . Is there any way to perform both operation with a single step/Click event .






Solution

No, there is no single step option.


Only possibility is directly click on upload button, then it automatically asks for save, if the document is modified click on "Yes" button to save and upload.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 002-8016506

KB Article ID# PL8016506

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC