Customize setting files for multiple STEP export in the same NX session

2021-10-06T23:27:33Z

Summary


Details

How do you customize settings file for each STEP export interactively in the  same NX session?
 AP103, AP214, AP242.



Solution

 The customer defaults allows to set settings file for only one Application protocol. But there is another way user can customize the settings file for each step export.

 Please set following environment variables (or set them in the NX Command Prompt window before launching NX) :

set NX_STEP203UG_EXPORT_DEF=D:\temp\PRs\step\test203.def - for STEP203 translator (for export) 
set NX_STEP214UG_EXPORT_DEF=D:\temp\PRs\step\test214.def - for STEP214 translator (for export) 
set NX_STEP242UG_EXPORT_DEF=D:\temp\PRs\step\test242.def - STEP242 translator (for export) 

You can get more information in the documentation under: 

Home -> Data Translation -> Data Translator -> Specifying a settings file using an environment variable 



Notes and References


Hardware/Software Configuration

Platform: na
OS: all
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V1847
Function: USER_INTERFACE

Ref: 001-9647202

KB Article ID# PL8016501

Contents

SummaryDetails

Associated Components