NX Unable to open an assembly after installing NX 12.0.2 MP13 with Teamcenter 10.1.7.1

2021-10-07T00:08:46Z
NX for Design

Summary


Details

Affected Software: NX 12.0.2
Affected Build(s): Maintenance Pack 13 (MP13)
Associated PR Number(s): 9644154
Resolved in Maintenance Pack: NX 12.0.2 MP14
Teamcenter specific Release: Teamcenter 10.1.7.1
 
 
Problem:
 
Unable to open an assembly after installing NX 12.0.2 maintenance pack 13 (NX 12.0.2 MP13) when used in combination with Teamcenter 10.1.7.1.  The problem reproduces when NX is used with Teamcenter Dispatcher. The problem is expected to reproduce on any Teamcenter 10.1.7 patch level.
 
When opening an assembly, the following error occurs:
 
Could not open ...
The following files could not be loaded, causing this open to fail:
"assyname" - The requested SOA object property is not loaded.
 
The log file shows the following errors:
 
+++ Property not loaded in object of type class UGS::PDM::Model::CDM::BomLine BOM::77253 : The property fnd0bl_configured_out is not defined for the type BOMLine.
+++ The requested SOA object property is not loaded
 
 
Solution:
 
The problem is resolved in NX 12.0.2 maintenance pack 14 (NX 12.0.2 MP14).
 
There is no workaround for NX 12.0.2 MP13 when used with Teamcenter 10.1.7 at any patch level.
 

SFB-NX-8016500
Product Information:
  • Product: NX , Application: NXMANAGER , Version: V12.0.2

KB Article ID# PL8016500

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX