NX is available for download

2021-10-07T00:08:45Z

Summary


Details


Dear Siemens Digital Industries Software Customer,
   
We are pleased to inform you that the latest product release of NX is now available for download from the Siemens Digital Industries Software download server.
 
Note: This is a full release and requires an update to the license file and the license server.
   
   
Download of NX on Windows 64-bit
   
Please use the following steps to download the NX product release and its documentation.
 


  • From the Download page, enter "SiemensNX-1899_wntx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages. 


  • Alternatively, the NX product release can be found using file navigator by entering NX into the Product Filter Feature on the left of your browser and then navigating through the NX directory structure as follows:


  • Expand the "NX" folder
  • Expand the "NX 1899 Series" folder
  • Expand the current release folder (NX 1899)   


 
Note:  When an NX series is replaced by a newer version, the previous version will be moved to the "NX Support" folder.  For example, when NX 1899 is replaced it can be downloaded as follows:
 
  • Expand the "NX Support" folder 
  • Expand the "NX Supported" folder 
  • Expand the "NX1899 Series" folder
  • Expand the available release name 
 
To download the NX product:


  •  Right click on the Release Package files
  •  Select "Save Target As" or "Save Link As" to save the files to your local destination 
 
File to download:
  
  • SiemensNX-1899_wntx64.zip 


Please refer to the readme file with the download for instructions on extracting the main zip file.
  


To download the NX documentation: 


  • Expand the "NX" folder 
  • Expand the "NX 1899 Series" folder 
  • Expand the "Documentation" folder 
  • Right click on the product documentation link 
  • Select "Save Target As" or "Save Link As" to save the file to your local destination  


In all cases, please refer to the supplied README file for installation instructions. 
    
More information regarding this NX release can be found in the following help topics:
  










Download of NX on Linux 64 – NX Batch
   
Interactive NX is no longer supported on Linux.  The product NX Batch runs in batch mode on the Linux Operating System.    
 


  • From the Download page, enter "nxbatch-1899_lnx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages.


  • Alternatively, the NX product release can be found using file navigator by entering NX into the Product Filter Feature on the left of your browser and then navigating through the NX directory structure as follows: 


  • Expand the "NX Batch" folder
  • To download the NX product:
  • Right click on the Release Package files 
  • Select "Save Target As" or "Save Link As" to save the files to your local destination
  • File to download: 
    • nxbatch-1899_lnx64.tar.gz


Please refer to the readme file with the download for instructions on extracting the main gz file.
  

To download the NX documentation:


  • Expand the "NX Batch" folder
  • Expand the "Documentation" folder
  • Right click on the product documentation link 
  • Select "Save Target As" or "Save Link As" to save the file to your local destination  


 
If you encounter any problems during this installation, please contact your local Siemens Digital Industries Software support.
   
For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:
     
http://www.plm.automation.siemens.com/en_us/products/nx/
http://support.industrysoftware.automation.siemens.com/gtac.shtml
 
 
Sincerely,
 
 
Siemens Digital Industries Software 



SFB-NX-8016481
Product Information:
  • Product: NX

KB Article ID# PL8016481

Contents

SummaryDetails

Associated Components