The Solid Edge Embedded Client (SEEC) [Teamcenter Integration for Solid Edge] is not pulling or downloading all linked documents.
The customer works with structured parts with different part copies.
e.g. draft - - part1 - Part Copy part 2 - Part Copy part 3
If the customer opens the draft through SEEC only the first part will be copied to the cache. You will then have strong edges on the view borders of the draft.
If you search the part copies in Teamcenter (Part Copy part1, Part Copy part 2) and open these write protected, the draft is up to date and no borders indicating that the view is out of date can be seen.
Is it possible to set an appropriate option to load the complete structure? If yes, what is the Option?
Solution
Yes this is possible by using the Download options in the file open dialogue. Select the "Download linked documents" and/or "Download linked drawings" to change this behavior.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC
Ref: 001-9648815