With an non-associativ measurement the size of the annotation does not adapt

2021-10-06T23:27:32Z

Summary


Details

When zooming in and zooming out on a part, although the option "delay Geometry, Expression, and PMI Update" is disabled,  NX cannot adapt the size of the annotation when zooming in or out.

Solution

This is a normal behavior. The tracking and management of non-associative annotations was not part of the original measurement design, and as such there is no current mechanism to update the size of the annotation as the display changes.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: NX
Application: DESIGN
Version: V12.0.1
Function: INFO_ANALYSIS

Ref: 002-8016434

KB Article ID# PL8016434

Contents

SummaryDetails

Associated Components