NX The status of active Components and of Form elements is unknown in Assembly with Wave Links

2021-10-06T23:27:32Z
NX for Design

Summary


Details

Cases:
1. Open Assembly with load options "Component fully" and any Reference Set
-> Status of active Component is OK

2. Open Assembly with load options "Component partially" and Reference Set "Model"
-> Status of active Component is unknown 
-> Status of Form elements is unknown
->  If working on Wave-Objects no Objects existing

3. Open Assembly with load options "Component partially" and Reference Set "Entire Part"
-> Status of active Component is unknown 
-> Status of Form elements is unknown
-> If working on Wave-Objects Objects are existing 
-> When working on it the Status is OK
 -> If you end the action with OK the Status will be changed to unknown.
 -> If changing any Option to active and the to inactive the status will be OK 

Common problem for these examples:
Status of active Components is unknown 
Status of Form elements is unknown



Solution

In general, if the source part of the links is not fully loaded, the linked part will be presented as Unknown in the assembly navigator, and the links will be shown as Unknown in the part navigator. 



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: NX
Application: ASSEMBLIES
Version: V12.0.2
Function: WAVE

Ref: 002-8016433

KB Article ID# PL8016433

Contents

SummaryDetails

Associated Components

Assemblies