Details
A piece part (not assembly part) in Teamcenter has an associated BVR; when this BVR is viewed in Structure Manager, the BOMLine has various objects such as Body, Sketch, Datum, Point, Edge, Face, Expression.
This piece part contains Product Interface, and it appears BVR is tracking those product interface outputs.
Is there a way to eliminate Teamcenter creating BVR to track Product Interface output?
Solution
This is due to customer defaults setting: Teamcenter Integration > General > Feature tab: Product Interfaces
This option determines whether or not product interfaces and their related engineering relations, such as WAVE links, inter-part expressions, and constraints, will be published to Teamcenter. When turned on at the time of saving a part containing product interfaces, the part will be treated as an assembly part with all product interfaces as child components. This will allow the product interfaces to participate in the querying, browsing, visualizing and consuming functionality in Teamcenter.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: ASSEMBLY
Ref: 002-8016376