Get Area Properties with dimensionable Centroid

2021-10-06T23:56:32Z

Summary


Details

Is there a way to get the Area Properties of a face with a Centroid that can be dimensioned to? 

Solution

Yes. Go to Inspect > Area > Select the Area. Click on the Area Properties button on the command  bar, followed by the green check mark > OK. This will place the Centroid in the view, which can be dimensioned to.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 2016
Product: SOLID_EDGE
Application: DRAFT
Version: V220MP2
Function: TOOLS

Ref: 001-9643358

KB Article ID# PL8016360

Contents

SummaryDetails

Associated Components