NX STEP 242 and tessellation option accuracy

2021-10-06T23:27:32Z
NX for Design

Summary


Details

When you translate a NX model to STEP AP242 there is a "Tessellated" option, ("Precise" is default), in the Export to STEP menu, Data to Export tab, "Export Solids and Surfaces as"


What is the accuracy for such tessellation?



Solution

The values being used to define the accuracy of the geometry being generated by NX to STEP242 translation with the "Tessellated" option is:
Chordal tolerance - 0.127 mm (0.005 inch)
Angular - 15 degrees
   where chordal tolerance is defined as how closely the triangles approximate the surface or solid and angular tolerance the is defined as upper bound of angular deviation between two surfaces normal.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: TRANSLATOR
Version: V1872
Function: STEP_AP242

Ref: 001-9636610

KB Article ID# PL8016349

Contents

SummaryDetails

Associated Components

CAD Translators