RobotExpert Controllers for ABB, COMAU, FANUC, KAWASAKI, KUKA, YASKAWA

2021-10-07T00:14:54Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that RobotExpert controllers for "ABB, COMAU, FANUC, KAWASAKI, KUKA, YASKAWA" are available for download from https://download.industrysoftware.automation.siemens.com.


   See RobotExpert_Controller_Name_changes_log.htm for details concerning this update.
   Note: This file is located in the 'Change_Logs' folder directly under the 'Robot_Controllers' folder.



Use the following steps to download.


Note: A valid WebKey account is required.
(URL: https://www2.industrysoftware.automation.siemens.com/webkey)


In your browser address window enter the URL: https://download.industrysoftware.automation.siemens.com/


WebKey Username: [your WebKey user ID]


WebKey Password: [your WebKey password]


Select the Download tab


In the Product Filter area scroll down to Tecnomatix Products
Select Tecnomatix Products
Expand Product updates
Expand RobotExpert/
Expand Robot_Controllers/
Expand V14.0/, V14.1/, V14.1.1/, V14.1.2/, V15.0/, V15.0.1/, V15.0.2/ or V15.1/
Expand ABB, COMAU, FANUC, KAWASAKI, KUKA or YASKAWA


Download the file(s):


    RobotExpert_14.0_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_14.0_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_14.0_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_14.0_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_14.0_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_14.0_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_14.1_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_14.1_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_14.1_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_14.1_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_14.1_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_14.1_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_14.1.1_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_14.1.1_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_14.1.1_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_14.1.1_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_14.1.1_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_14.1.1_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_14.1.2_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_14.1.2_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_14.1.2_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_14.1.2_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_14.1.2_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_14.1.2_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_15.0_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_15.0_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_15.0_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_15.0_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_15.0_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_15.0_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_15.0.1_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_15.0.1_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_15.0.1_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_15.0.1_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_15.0.1_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_15.0.1_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_15.0.2_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_15.0.2_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_15.0.2_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_15.0.2_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_15.0.2_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_15.0.2_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe



    RobotExpert_15.1_ABB_RAPID_64BIT_v3.40_29_11_2019.exe
    RobotExpert_15.1_COMAU_PDL_64BIT_v4.8.4_29_11_2019.exe
    RobotExpert_15.1_FANUC_RJ_64BIT_v2.69_29_11_2019.exe
    RobotExpert_15.1_KAWASAKI_AS_64BIT_v3.5.1_29_11_2019.exe
    RobotExpert_15.1_KUKA_KRC_64BIT_v4.6_29_11_2019.exe
    RobotExpert_15.1_YASKAWA_INFORM_64BIT_v4.47_29_11_2019.exe




To Install:


Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the RobotExpert installation).


Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.


The default installation point is C:\Program Files\Tecnomatix.



If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.


Sincerely,


Siemens Digital Industries Software

SFB-TECNOMATIX-8016344
Product Information:
  • Product: TECNOMATIX , Application: ROBOTEXPERT

KB Article ID# PL8016344

Contents

SummaryDetails

Associated Components