Background information on Engineering Reference terms

2021-10-06T23:56:31Z

Summary


Details

For the Engineering Reference is there some background information available about the terms that are used inside the application for the input and the calculated values?  For example, in the bevel gear generator the terms "tooth thickness coefficient" and the "roughness factor" are used.



Solution

The Engineering Reference uses data from the various engineering standards to create the geometry.

If you need further background information on the various terms and what they mean then you should review the relevant engineering standard.

All of the standards used in Engineering Reference are documented in the Solid Edge Help system under each relevant section of the Engineering Reference help:

http://docs.plm.automation.siemens.com/tdoc/se/2020/se_help#uid:xid1129777:xid1323753:index_xid718565

For example, you mention bevel gears, here is the link to the various standards used to create those bevel gears in Engineering Reference:

http://docs.plm.automation.siemens.com/tdoc/se/2020/se_help#uid:xid1129777:xid1323753:index_xid718565:xid721875:xid719643




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V220.0
Function: ENGR_REFERENCE

Ref: 002-8016326

KB Article ID# PL8016326

Contents

SummaryDetails

Associated Components