Deploying Preferences file in silent install of Solid Edge

2021-10-06T23:56:30Z

Summary


Details

Is there a way to deploy a Preferences file as part of a Solid Edge silent install when deploying Solid Edge to all users?

Solution

There is no way to explicitly specify a Solid Edge preferences file to deploy as part of the initial base Solid Edge installation. However, the Settings and Preferences Wizard does provide a command line interface.

Therefore in order for acustomer to deploy their Solid Edge preferences silently, the customer simply needs to add another line to their install script to call the Settings and Preferences Wizard command line.

For more on the command line options available with the Settings and Preferences Wizard please see the following documentation:

http://docs.plm.automation.siemens.com/tdoc/se/2020/se_help#uid:xid1129777:xid1325276:xid1325280:index_customize_solid_edge:xid1186097:xid1186145





Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V220.0
Function: INSTALL

Ref: 002-8016325

KB Article ID# PL8016325

Contents

SummaryDetails

Associated Components