After running
Tool Path -> Verify on an
Operation the
Analyze utility is run. Though the output motion from a circle record is correct
Analyze reports that there are gouges. Why are these gouges being displayed?
NX shows a .0009 deviation on the arc move when
Analyze is run.

In contrast, notice that a linear move shows 0 deviation.

Solution
The Tool
Path -> Verify -> Analyze utility is intended to be used as an approximate overview. This is caused by the built-in accuracy limitations of a faceted
IPW. The
Gouge Check utility is much more accurate and is the suggested mechanism to use for this report.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1888
Function: VERIFY
Ref: 002-8016271