Clients may desire the ability to control the default Snap Point options enabled and have them be persistent from session to session.

Solution
There is no Customer Default (or such) support for snap point options.
Snap Point toggle states do, however, participate in the Dialog Memory mechanism. So if I launch Point, for example, and set my toggles, their states are remembered for the next launch of that command, even across NX sessions.
Note: Toggle states (and filters,) are generally only stored in Dialog Memory when the command is completed with OK, not Cancel.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSENG
Version: V1899
Function: SELECTION
Ref: 001-9634907