Prevent SEEC from creating multiple draft datasets

2021-10-06T23:56:29Z

Summary


Details

How to prevent multiple SE Draft datasets from being created on an Item Revision?



Solution

In Solid Edge 2020 we added a new TC preference SEEC_Draft_GRM_Rule.   This preference determines the maximum number of Solid Edge Draft datasets that can be attached to the revision. 

The value should be equal to the value defined in BMIDE for GRM Rule for SE Draft. A value of -1 indicates no limit. Valid values are -1 or a positive integer



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 001-9632959

KB Article ID# PL8016219

Contents

SummaryDetails

Associated Components