The posted code file needs to have the G_adjust and H words output in the initial rapid move for each operation so the operator has safe restart codes in place at every operation.
Solution
The best option for this is to add the G_adjust and H words to the standard 'force addresses' custom command in start of path:

These words are usually included in the force addresses command in the tool change event, but if the tool is repeated, this force command is not being read (since the tool change event is being bypassed). Adding them to the overall start of path event forces them out at the start of every operation, whether there is a tool change or not.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V11.0.2
Function: POSTBUILDER
Ref: 002-8016209