AtTI: How to add the Solid Edge assembly configuration file to Teamcenter

2021-10-06T23:56:28Z

Summary


Details

Using SEEC and AtTI products, how do you add the Solid Edge assembly's .cfg file to Teamcenter.



Solution

The .cfg file is automatically uploaded with the .asm file. The cfg is saved when the asm is saved and both are uploaded together. The files are located in the ItemRev -> Name Reference menu as seen via the Teamcenter RAC interface.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1507
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: P219MP10
Function: SEEC

Ref: 001-9630225

KB Article ID# PL8016173

Contents

SummaryDetails

Associated Components