Solid Edge Parasolid version for the current Solid Edge version

2021-10-06T23:56:27Z
PART/SHEETMETAL TRANSLATORS

Summary


Details

How to determine the Parasolid version information for the currently installed Solid Edge version?

Solution

The Parasolid version information can be found in the Solid Edge "readme.HTM" file which is located in the Solid Edge installation folder e.g. the default location: "C:\Program Files\Siemens\Solid Edge Version". 

For example, the Solid Edge 2020 readme.htm file contains the information about the current and also the previous Solid Edge versions. 

Solid Edge version 2020 = Parasolid version 31.1 
Solid Edge version 2019 = Parasolid version 30.1 
Solid Edge version ST10 = Parasolid version 30.0
...
 
For other previous Solid Edge versions please check the readme.htm file 





Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V220.0
Function: INSTALL
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V220.0
Function: PARASOLID

Ref: 002-8016159

KB Article ID# PL8016159

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES