When the tool diameter is the same size as the slot...the plunge milling operation is to cut down the slot center. The tool path cuts down the center and then recuts some of the previously machined slot.
TARGET PARTSTOCK PARTCUT AREA
Solution
- Define the "WORKPIECE" with the "BLANK" defined. Do not "Specify the Part" in the "Workpiece".
- Specify the "Part" inside of the Operation.
- Select the "Floor" and "Side Wall" of the slot as the "Part" (please see image below).
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1888
Function: PLUNGE_MILLING
Ref: 002-8016132