Start Diameter in Hole Milling

2021-10-06T23:27:31Z

Summary


Details

The "Start Diameter" is not populating with the IPW hole diameter. The previously drilled hole was .120 diameter. The "Feature Geometry" shows "Start Diameter" of 0.000.


The image below shows a "Clip Section" of the part.

The "Point Length" of the tool is .0248.




Solution

To auto-populate the "Start Diameter" , "Bottom Stock"  must be greater than the "Point Length"  of the drilled hole. In this example:

Drill parameters in the image below...


Notice that the "Point Length"  is .0248

The "Feature Geometry" Cutting Parameters, Bottom Stock must be greater than the "Point Length"  in order to auto-populate the "Start Diameter" as seen in the image below.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1888
Function: HOLE_BOSS_MILL

Ref: 002-8016101

KB Article ID# PL8016101

Contents

SummaryDetails

Associated Components