NX DOCUMENTATION ER ---- NX1888 - SE2020 compatibility

2021-10-06T23:27:30Z
NX for Design

Summary


Details

do you have information which NX version and when will be compatible with SE2020 ?
NX 1888 is not able to open an SE 2020 par.
Error Message is :==================Could not open se2020.par
The following files could not be opened, causing this open to fail
se2020.par -Part file is from a newer version of NX than the one supported by NX


Solution

The Problem depends on the Parasolid Version behind.SE2020 uses Parasolid V32.0 and NX1888 uses Parasolid V31.1
So you will not been able to open this SE part in NX.
Solution is to install NX1899 (end of the Year) , this has also the Parasolid Version 32.0 behind.


Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1903
Product: NX
Application: ASSEMBLIES
Version: V1888
Function: PART_FILE_OPS

Ref: 001-9620736

KB Article ID# PL8016046

Contents

SummaryDetails

Associated Components

Assemblies