Solid Edge 2020 - Maintenance Pack 2 Announcement

2021-10-07T00:10:02Z

Summary


Details

October 31, 2019
 
Dear Solid Edge Customer: 
 
Solid Edge 2020 Maintenance Pack 2 is now available for download.
 
We appreciate your continued business and your participation in the software support process - - your reporting helps us make Solid Edge more productive for the way you do business.
 
Sincerely,
The Solid Edge Team 
 
============
Release Notes:
============
 
Solid Edge 2020 MP2
Version: 220.00.02.10
 
Solid Edge 2020 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
 
Solid Edge 2020 Maintenance Pack downloads area:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/2020/Maintenance_Packs/
 
Our policy on Maintenance Packs -- we release Maintenance Packs for CRITICAL items only. Maintenance Packs are available up to a maximum of 15 months following the release date. The release date for Solid Edge 2020 was 07/19/2019, making the Maintenance Pack cutoff date 10/19/2020.
 
===============
E-mail Notification: 
===============
 
Plug-in to the electronic advantage by subscribing to our e-mail distribution services. This service keeps you informed of pertinent technical information automatically and in a timely manner using electronic mail. To receive direct e-mail notifications for Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
 
   https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
============================================
This Maintenance Pack addresses the following PRs:
============================================
 
===General===
PR 9562554: 3YourMind service page is not able to display
 
===API===
PR 9578103: Need an API function for a specified ribbon tab activation
 
===Assembly=== 
PR 9562441: ST5 Assembly will not open after installing the latest Windows 10 Update
PR 9410937: Assembly file being too large even with no components in it
PR 9593019: Activate command from the ribbon with a large number of parts selected is slow
PR 9604738: Strange faces in KeyShot when converting from Solid Edge
 
===Draft=== 
PR 9521310: Impossible to convert a DFT in DWG
PR 9522595: Text box justification/indent settings
PR 9582996: Edge crashes doing forced update on this drawing.
PR 8430769: Unable to make change in text and save - OK is grayed out
 
===Part/Profile/Sheet Metal===
PR 9534819: slow sketch commands when using styles
PR 9574007: Bug with Ordered dimension
PR 8420018: Not able to modify driving dimensions 
PR 9584163: Cannot Lock and adjust a dimension in the sketch profile as expected
 
===Teamcenter Integration for Solid Edge===
PR 8428611: Download linked documents causes all FOP members to be downloaded to cache
PR 9577043: ATTI closes when importing assembly
PR 9573746: Need to prevent an empty query on SEEC 
PR 9577671: Solid Edge crashes when expanding an assembly opened with Hide All
PR 9539084: Active Workspace 4.2 in SEEC Drag and Drop does not work
 
===Translators===
PR 9550202: When exporting to DXF with All sheets to same file some dimensions are duplicate
PR 9577689: CAD properties disappear when converted to JT file
 

SFB-SOLID_EDGE-8016033
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8016033

Contents

SummaryDetails

Associated Components