NX Cannot Add an SE2020 Component File to an NX1888 CAM Assembly

2021-10-06T23:27:30Z
NX for Manufacturing

Summary


Details

An error is displayed when attempting to load a Solid Edge SE2020 Component file into an NX1888 CAM Assembly. Why is this message displayed?



Solution

The Parasolid Kernel version used in SE2020 is from a newer version than the one in NX1888. NX and SE2020 will become compatible when the NX1899 version is released. An XML update file for this can be downloaded using the link below.


https://download.industrysoftware.automation.siemens.com/download-n.php/solid_edge/product_updates/2020/PLMXML/V220.0.zip



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1888
Function: PART_CONVERSION

Ref: 001-9616106

KB Article ID# PL8015989

Contents

SummaryDetails

Associated Components

Manufacturing General