Unable to save a post processor from Post Builder after making changes because Post Builder found a tcl error in an older VNC command:

Solution
The error message names the variable "mom_sim_num_machine_axes" variable in the PB_CMD_vnc__preprocess_nc_block command. A study of this custom command shows that this variable is used in an 'if' test, but was never declared.
At the top of the command, just under the introductory comments block, add a global declaration of this variable, alongside all the other declarations that already exist:
global mom_sim_num_machine_axes
Attempting to save the post after this change revealed the same error for another variable in this custom command. Add a similar declaration for the "mom_sim_mt_axis" variable, so the resulting additions to the declaration list looks like this:

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V12.0.2
Function: POSTBUILDER
Ref: 002-8015976