Posted output to contain a user defined number of points on a line.
NC Output with Planar Mill OperationTOOL PATH/PLANAR_PROFILE,TOOL,EM.500
TLDATA/MILL,0.5000,0.0000,3.0000,0.0000,0.0000
MSYS/0.0000,0.0000,0.0000,1.0000000,0.0000000,0.0000000,0.0000000,1.0000000,0.0000000
$$ centerline data
PAINT/PATH
PAINT/SPEED,10
PAINT/COLOR,31
FEDRAT/IPM,10.0000
GOTO/15.0000,-0.2500,0.0000,0.0000000,0.0000000,1.0000000
GOTO/0.0000,-0.2500,0.0000
PAINT/SPEED,10
PAINT/TOOL,NOMORE
END-OF-PATH
The above NC output displays a GOTO at the start of the line and a GOTO at the end of the line.
The desire is to have a GOTO output every .150".
Solution
- Using the existing line, extrude a sheet body. The operation calls for a .500 diameter end mill. The extrusion is offset .250 from the intended cutting edge. (The line below is 15 inches long.)

- Create a Fixed Contour Operation.
- Do not select Part, Check, or Cut Area.
- In the "Drive Method", select "Surface Area".

- Specify the Drive Geometry by selecting the "Sheet Body".
- Set the "Cut Area" to "Surface %".

- Select the cut direction as indicated in the image below...

- Change the "Surface %" to cut along one side of the surface.

- Please see the image below to set the "Drive Settings".

Note: The "Contact Points" should display as seen below...

- Select "OK" on the "Surface Area Drive Method" dialog box.
- Generate.
Note: The Tool Path outputs the desired amount of "GOTO".
TOOL PATH/FIXED_CONTOUR,TOOL,EM.500
TLDATA/MILL,0.5000,0.0000,3.0000,0.0000,0.0000
MSYS/0.0000,0.0000,0.0000,1.0000000,0.0000000,0.0000000,0.0000000,1.0000000,0.0000000
$$ centerline data
PAINT/PATH
PAINT/SPEED,10
PAINT/COLOR,31
FEDRAT/IPM,10.0000
GOTO/15.0000,-0.2500,0.0000,0.0000000,0.0000000,1.0000000
GOTO/14.8500,-0.2500,0.0000
GOTO/14.7000,-0.2500,0.0000
GOTO/14.5500,-0.2500,0.0000
GOTO/14.4000,-0.2500,0.0000
GOTO/14.2500,-0.2500,0.0000
GOTO/14.1000,-0.2500,0.0000
GOTO/13.9500,-0.2500,0.0000
GOTO/13.8000,-0.2500,0.0000
GOTO/13.6500,-0.2500,0.0000
GOTO/13.5000,-0.2500,0.0000
GOTO/13.3500,-0.2500,0.0000
GOTO/13.2000,-0.2500,0.0000
GOTO/13.0500,-0.2500,0.0000
GOTO/12.9000,-0.2500,0.0000
GOTO/12.7500,-0.2500,0.0000
GOTO/12.6000,-0.2500,0.0000
GOTO/12.4500,-0.2500,0.0000
GOTO/12.3000,-0.2500,0.0000
GOTO/12.1500,-0.2500,0.0000
GOTO/12.0000,-0.2500,0.0000
GOTO/11.8500,-0.2500,0.0000
GOTO/11.7000,-0.2500,0.0000
GOTO/11.5500,-0.2500,0.0000
GOTO/11.4000,-0.2500,0.0000
GOTO/11.2500,-0.2500,0.0000
GOTO/11.1000,-0.2500,0.0000
GOTO/10.9500,-0.2500,0.0000
GOTO/10.8000,-0.2500,0.0000
GOTO/10.6500,-0.2500,0.0000
GOTO/10.5000,-0.2500,0.0000
GOTO/10.3500,-0.2500,0.0000
GOTO/10.2000,-0.2500,0.0000
GOTO/10.0500,-0.2500,0.0000
GOTO/9.9000,-0.2500,0.0000
GOTO/9.7500,-0.2500,0.0000
GOTO/9.6000,-0.2500,0.0000
GOTO/9.4500,-0.2500,0.0000
GOTO/9.3000,-0.2500,0.0000
GOTO/9.1500,-0.2500,0.0000
GOTO/9.0000,-0.2500,0.0000
GOTO/8.8500,-0.2500,0.0000
GOTO/8.7000,-0.2500,0.0000
GOTO/8.5500,-0.2500,0.0000
GOTO/8.4000,-0.2500,0.0000
GOTO/8.2500,-0.2500,0.0000
GOTO/8.1000,-0.2500,0.0000
GOTO/7.9500,-0.2500,0.0000
GOTO/7.8000,-0.2500,0.0000
GOTO/7.6500,-0.2500,0.0000
GOTO/7.5000,-0.2500,0.0000
GOTO/7.3500,-0.2500,0.0000
GOTO/7.2000,-0.2500,0.0000
GOTO/7.0500,-0.2500,0.0000
GOTO/6.9000,-0.2500,0.0000
GOTO/6.7500,-0.2500,0.0000
GOTO/6.6000,-0.2500,0.0000
GOTO/6.4500,-0.2500,0.0000
GOTO/6.3000,-0.2500,0.0000
GOTO/6.1500,-0.2500,0.0000
GOTO/6.0000,-0.2500,0.0000
GOTO/5.8500,-0.2500,0.0000
GOTO/5.7000,-0.2500,0.0000
GOTO/5.5500,-0.2500,0.0000
GOTO/5.4000,-0.2500,0.0000
GOTO/5.2500,-0.2500,0.0000
GOTO/5.1000,-0.2500,0.0000
GOTO/4.9500,-0.2500,0.0000
GOTO/4.8000,-0.2500,0.0000
GOTO/4.6500,-0.2500,0.0000
GOTO/4.5000,-0.2500,0.0000
GOTO/4.3500,-0.2500,0.0000
GOTO/4.2000,-0.2500,0.0000
GOTO/4.0500,-0.2500,0.0000
GOTO/3.9000,-0.2500,0.0000
GOTO/3.7500,-0.2500,0.0000
GOTO/3.6000,-0.2500,0.0000
GOTO/3.4500,-0.2500,0.0000
GOTO/3.3000,-0.2500,0.0000
GOTO/3.1500,-0.2500,0.0000
GOTO/3.0000,-0.2500,0.0000
GOTO/2.8500,-0.2500,0.0000
GOTO/2.7000,-0.2500,0.0000
GOTO/2.5500,-0.2500,0.0000
GOTO/2.4000,-0.2500,0.0000
GOTO/2.2500,-0.2500,0.0000
GOTO/2.1000,-0.2500,0.0000
GOTO/1.9500,-0.2500,0.0000
GOTO/1.8000,-0.2500,0.0000
GOTO/1.6500,-0.2500,0.0000
GOTO/1.5000,-0.2500,0.0000
GOTO/1.3500,-0.2500,0.0000
GOTO/1.2000,-0.2500,0.0000
GOTO/1.0500,-0.2500,0.0000
GOTO/0.9000,-0.2500,0.0000
GOTO/0.7500,-0.2500,0.0000
GOTO/0.6000,-0.2500,0.0000
GOTO/0.4500,-0.2500,0.0000
GOTO/0.3000,-0.2500,0.0000
GOTO/0.1500,-0.2500,0.0000
GOTO/0.0000,-0.2500,0.0000
PAINT/SPEED,10
PAINT/TOOL,NOMORE
END-OF-PATH
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V12.0.2
Function: SURFACE_CONTOUR
Ref: 002-8015962