Solid Works does not run after installing Solid Edge on the same machine.

2021-10-06T23:56:24Z

Summary


Details

Solid Works 2018 SP3 is aborting after installing Solid Edge 2020 on the same machine.



Solution

The problem reported was that, Works comes up and runs for about 10 to 15 minutes and then crashes. The problem has been isolated to .net version 4.6.2 which is required by Solid Edge and which Solid Works is not compatible with.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: SETUP
Version: V220MP1
Function: INSTALL

Ref: 001-9609708

KB Article ID# PL8015939

Contents

SummaryDetails

Associated Components