Saving a file will report that the Property Find No. is not modifiable

2021-10-06T23:27:30Z

Summary


Details

The assembly is failing to save with the following message:
======================================
The following objects failed to save:
While saving ItemID/ItemRev - ItemName:ItemID/ItemRev - ItemName - while saving product structure data to Teamcenter: Property Find No. is not modifiable.
<<OK>>
======================================



Solution

This can be resolved by changing the value of the Teamcenter preference:
   PS_Duplicate_FindNo_Update
This preference deals with whether or not duplicate find number values are allowed in certain cases on multiple instances of the same child part in a given parent. If the same find number assigned to multiple instances of the same part in a parent is needed, this site preference should be set to "true" to make sure that such assemblies successfully save.
In Teamcenter, go to 'Edit-->Options' and change this preference. Then re-start both Teamcenter and NX.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_SAVE

Ref: 001-9606011

KB Article ID# PL8015937

Contents

SummaryDetails

Associated Components